AXIS#.IL.KP

Description

AXIS#.IL.KP is used to read the proportional gain of the PI-loop that controls the q-component of the current.

The value is Read-Only, and is changed by modifying the current loop bandwidth setting (AXIS#.IL.BW).

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read Only

Units

V/A

Range

0 to 2,000 V/A

Default Value

N/A

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.KP

500ah

02h

Unsigned32

-

1000:1

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5819

1

5819 (0x16bb)

AXIS1.IL.KP

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS1.IL.KP

5819

Float

Read Only

-